Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Can I upgrade Automation Server classic (AS) to EBO V3.2 or higher?
Issue:
Need to upgrade EBO project to V3.2 or higher but I have Classic Automation Server (AS)

Environment:
EcoStruxure Building Operation

Resolution:
EBO V3.2 or higher releases are not supported on the original AS’s often referred to as AS classic. From version 3.1 of EcoStruxure BMS it is possible to use a multi-version system, so you can keep AS to EBO V3.1.2 and upgrade other a servers (EC, ES, AS-P and AS-B) to EBO V3.2 or higher. Check below architecture as example: