Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
SP-C controller doesn't reply to ping request
Issue:
SP-C controller is online but doesn't reply to ping request.

Environment:
EcoStruxure Security Expert, SP-C

Resolution:
As a Cybersecurity enhancement, ping is disabled by default for the onboard Ethernet connection on SP-C with firmware V2.08.825 or higher. It can be re-enabled via Controller Commands. You can also check SP-C online status on the Security Expert software or via the SP-C web interface.