Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to calculate “Tt Timing setting accuracy” of RM17TE00 product?
The RM17TE00 product’s Tt timing setting is +/-10% (full scale).

Example:

When the Tt setting is configured to 5s, the actual time delay is 5s +/-10% of the full-scale value.

Actual Time Delay, Tt = 5s +/- (10% x 10s) = 5s +/-1s