Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the single phase Altivar drives be used on single phase motors?

Article available in these languages: Spanish, SL

Issue:
Could not find a drive to work with a single phase motor.

Product Line:
Altivar Machines

Environment:
All models and serial numbers

Cause:
N/A

Resolution:
All AC drives sold by SquareD Schneider Electric in the US are for use with 3 phase motors only. The single phase units are for use with single phase input only.