Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does shielded motor cable have to be grounded on both ends or just one when used with an Altivar AC drive?
Issue:
Installation inquiry for the shielded motor cable on an Altivar AC drive

Product Line:
Altivar Drives

Environment:
All

Cause:
Proper grounding

Resolution:
Shielded motor cables need to have the shield wire grounded at both ends of the shielded cable.  See figure 13 (Rule 2) in the Grounding and Bonding Practices when Installing Variable Frequency Drives manual document 8800DB1501.

shielded cable