Issue:
Need to know what 45mm, 54mm, and 72mm pitch means
Product Line:
GV2 Manual Starters
Environment:
IEC Contactors and Starters
Resolution:
The pitch is the spacing between slots. In order to select the correct pitch, total up the width of the device, plus any side mounted auxiliaries. Use the total width for selecting the proper pitch. The busbar pitch selection must be the same or greater than the sum of device and auxiliaries.
Released for: Schneider Electric Egypt and North East Africa