Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are 21 volt replacement control coils available for LC2D4011?
Issue:
LC2D4011 replacement coil

Prodcut Line:
IEC Contactors and Starters

Product Line:
TeSys™ D Contactors

Resolution:
21VAC coils are not an option on these reversing change over contactors.
We do offer the B6 or B7 which is 24VAC.  The tolerance on the 24V coil is 85 to 110%.  So the 24VAC coil will work down to 20.4VAC.

Note the LC2D4011 series is obsolete.