How can we help you today?

What is the part number of the spring mounting clips that attach to the box to install an I-Line trim that was provided between July 1994 and August 1997 and a current I-Line hinged trim?

Issue:
Part umber of the spring mounting clips that attach to the box to install an I-Line trim that was provided between July 1994 and August 1997 and a current  I-Line hinged trim.

Product Line:
I-Line Panelboards

Environment:
Installation

Resolution:
This is a 1/4-20 tinneman fastener and the part number is 23301-02203.


Schneider Electric Egypt and North East Africa
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
  • Help and Contact Center