How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

How to communicate with the Series 300 Group G controller via RS485?

You can communicate with the series 300 switches Group G controller via the RS-485 port if the ATS has the optional Accessory 11BE.

The Accessory 11BE is a four-function software bundle.  One of the four functions is to allow the user to configure the RS485 communications port.  Please see Group G Controller Users Guide .




The image below will show you the location of the RS485 port and the S7 & S8 dipswitches.




For the proper RS485 port terminal designations, please refer to the ATS wiring diagram.  For generic Series 300 Group G wiring diagrams, please click this link .

For 2-wire serial connection, set S8 dipswitch actuators over to the right (ON position), and choose to connect your two wires on either the Rx terminals or the Tx terminals.




If you're communicating via MODBUS, click this link for a copy of the MODBUS register map for the Series 300 Group G controller.

If unsure, contact Technical Support at 1-800-800-ASCO or send an email to technicalsupport@ascopower.com

You may also watch the videos related to this (please see below).




Schneider Electric Egypt and North East Africa
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
Help Center

Help Center