Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Where can I get pre and post-transfer signals on series 300 with Group G controller?
To have pre and post-transfer signals available, feature 31 needs to be enabled.

For Series 300, a set of form C contacts are provided on the group G controller as "OP1".



When the feature setting of "OP1" is set to operate the contacts as "Feature 31", the time delay settings of the pre and post-transfer signals are available.



For further information, refer to page 11 of the Group G controller user's guide.  If unsure, contact Technical Support at 1-800-800-ASCO or send an email to technicalsupport@ascopower.com