Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to select the LPCT/LPVT option (offline) in Easergy P3 through Easergy pro software?

!!!Confidential Content

Description/Issue :
Select the LPCT/LPVT option (offline) in Easergy P3 through Easergy pro software?


Environment/Product line:
Easergy P3 relays

Resolution :
Please follow this procedure in case you need create off-line settings to Easergy P3 with LPCT options.
1.    In the option 'X5' - Voltage Measurements + I/O option, should be selected the option 'C - 6DI + 3DO

000132810 2. After, Easergy Pro will be enabled the LPCT option on 'X1' - Phase Currents and voltage input as '7/8-for 3xLPCT+5xLPVT
000132810_2
After the above configure the device will support for LPCT/LPVT