Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
There is an issue in Modbus driver installation with SFT2841.Can you share the procedure to install SFT2841 works on Windows XP with driver Modbus version 1.14?
Issue:
There is an issue in Modbus driver installation with SFT2841.
Procedure need to install SFT2841 works on Windows XP with driver Modbus version 1.14

Environment/Product line:
Sepam relays

Resolution:
Please find attached the procedure for Modus driver installation to work with SFT2841 software & connect with Sepam relays properly .

Schneider Electric Egypt and North East Africa

Attachment(s)
SFT2841 on Windows XP Modbus driver 14.4 for windows XP.pdf [413.96 KB]
Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: