Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
BMXCRA312x0 and the BMECRA312x0 remote adapters 'Custom RPI' parameters settings does not work.
Custom RPI settings for the BMXCRA312x0 or BMECRA312x0 remote adapters do not work when using Unity V13.1, CE V14.0, or CE V14.1.

For example, if the RPI is set to 31ms in the following configuration,


The RPI does not display the change in the DTM.


The issue is resolved in:
  • Control Expert V15.0
  • Control Expert V14.1 using HotFix1 (HF1)

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center