Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to enable and configure Modbus TCP/IP on 5140/5170 QEM
For QEM using Firmware version 987204-022 or higher

Prerequisite:
1. QEM must be connected to the ASCO Controller.
2. QEM's IP address/Network settings should already be configured.

Enabling Modbus on QEM:
1. Login on the QEM web interface using the set IP address.
2. Go to Configuration tab > Ethernet Module

3. Click Edit and verify access. Use admin access to edit configuration,

4. On IPV4 tab, enable Modbus TCP IP and click Save.


Configuring Modbus on QEM:
> The QEM maps the Modbus data using the TCP/IP Alias table to define the device addressing.
> This is the device address needed when configuring the Modbus client.

1. On Ethernet Module Configuration page, go to Device List tab.

2. Change the Modbus Alias address to meet the site requirement. Click Save.

ASCO Modbus Register Maps document:
1. Group G controller - 381339-310
2. Power Manager XP (ASCO 5220) and Group 5 controller - 381339-221
3. Power Meter (ASCO 5210) - 381339-307

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center