Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to test the rectifier?
A bridge rectifier is composed of diodes. There are two ways to test a diode.

A. Through a Diode Test
First, make sure to disconnect the white wires and black wires from the bridge rectifier.
Then, You need to have your multi-tester dial set in Diode Test Mode. (dial setting no. 14)

image.png




image.png

image.png


B. For through Resistance Check,
You need to have your multi-tester dial set in Ohmmeter. (dial setting no. 12)

image.png

Then, check the resistance of each adjacent terminals.  (top & right/ top & left/ bottom & right/ bottom & left)
You should get a resistance reading of around 97 ohms or as long as all resistance readings are approximately the same, the rectifier is good.
image.png

If unsure, contact Technical Support at 1-800-800-ASCO or send an email to technicalsupport@ascopower.com