Is there a way to Freewheel Stop on Profinet with Process Drives?
Issue:
How can you do a freewheel stop on the ATV630 and ATV930 over Profinet command?
Product Line:
ATV630, ATV930 Series with Profinet option card.
Environment:
All
Cause:
Want the drive to freewheel stop when command is coming from the Profinet network.
Resolution:
CMD or command bits 0 and 1 both have set to 0 at the same time to command a freewheel stop over the Profinet network.
How can you do a freewheel stop on the ATV630 and ATV930 over Profinet command?
Product Line:
ATV630, ATV930 Series with Profinet option card.
Environment:
All
Cause:
Want the drive to freewheel stop when command is coming from the Profinet network.
Resolution:
CMD or command bits 0 and 1 both have set to 0 at the same time to command a freewheel stop over the Profinet network.
Released for: Schneider Electric Egypt and North East Africa