Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can Start and Stop be performed with an Analog signal on ATV212 drive?
Issue:
Can I start and stop the ATV212 drive with a 4-20ma analog signal?

Product Line:
ATV212

Environment:
All

Cause:
No Start Stop control signal on VFD

Resolution:
No. The start and stop (forward / reverse) commands should be controlled with digital inputs (+24Vdc only).

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center