Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many clients can be connected to the same server in the same time with Web Viewer of EcoStruxure Operator Terminal Expert?
The goal is this FAQ is to determine how many clients (using Web Viewer) can be connected in the same time on the same HMI.

This article is applicable for EcoStruxure Operator Terminal Expert V3.2 minimum.

3 simultaneous clients can be connected in the same time for HMIST6 Series and HMISTM6 Series.
5 simultaneous clients can be connected in the same time for HMIGTU and iPC.