Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why float type tags are not read correctly in EcoStruxure Machine SCADA Expert through OPCUA?
In some cases, the float type tags are not read correctly through OPCUA. A value on server like 12.345 is displayed on EcoStruxure Machine SCADA Expert as 12

The article is applicable for EcoStruxure Machine SCADA Expert 2020 minimum

The behaviour is visible only in computer in european environment. The comma is not reconized correctly.
To fix the issue, download and follow the step:

File: https://schneiderelectric.sharepoint.com/:u:/s/BoxSupportL3Group/EQDJl9WHNwNBqAbS_vY_bikBCWpnFptgtu_a8i07q1qpwA?e=QUBY1u
  1. Close and Stop any instance of EMSE.
  2. Unzip the folder.
  3. Rename the current file < OPCUAClient.dll > to < OPCUAClient_old.dll > into the folder: < C:\Program Files (x86)\........... >
  4. Copy/Paste the unzipped file (OPCUAClient.dll) on < Bin > folder

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: