Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is Feature 31 and how does it work with a Group G controller?

Feature 31 is a Selective Load Disconnect Feature. This is a standard feature that includes sub-features 31F, 31G, 31M, and 31N. One (1) set of form C contacts are provided on the Group G controller as “OP1”. When the contact “OP1” is set to operate as “Feature 31”, the time delay settings of the sub-features are available. If system requires more than one (1) set of contacts, an optional accessory 18RX can be added to provide an additional two (2) sets of form C contacts labeled "OP2" and "OP3".
Feature 31 and how does it work with a Group G controller
“OP1” can be set to operate to provide the following functions using the time delay setting associated with each sub-feature.

31F – Normal to Emergency Pre-Transfer signal
31G – Emergency to Normal Pre-Transfer signal
31M – Normal to Emergency Post-Transfer signal
31N – Emergency to Normal Post-Transfer signal

To program "OP1" to work as Feature 31,  the feature 31 needs to be set to "YES" under Feature settings of the Group G controllerFeature 31 and how does it work with a Group G controller
To set the time delay on Feature 31, on the controller navigate to Timer Settings and set desired time delay with an adjustment range of 0 – 5 min 59 secs.
Feature 31 and how does it work with a Group G controller
Refer to User’s Guide with manual number 381333-400 for additional setting information.

If unsure, contact Technical Support at 1-800-800-ASCO or send an email to technicalsupport@ascopower.com