Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What happens to Feature 2B (Time Delay Normal to Emergency N>E) and Feature 3A (Time Delay Retransfer to Normal E>N) if Feature 34A or 34B (Inhibit transfer) inputs are active in a Group 5 controller?

Feature 34A - Opening of the contact will prohibit transferring to the normal source
Feature 34B - Opening of the contact will prohibit transferring to the emergency source

Below are the simulations that were done to observe the operation of Feature 2B & Feature 3A when Feature 34 inhibit inputs are active.

TRANSFER NORMAL TO EMERGENCY

  • When 34B Contact Closed > Initiate Transfer N>E > TD N>E Countdown Running > Open Contact 34B > TD N>E Countdown Still Running > After Countdown Transfer Inhibited
  • -When 34B Contact Open > Initiate Transfer N>E > TD N>E No Countdown > Transfer Inhibited
TRANSFER EMERGENCY TO NORMAL
  • When 34A Contact Closed > Initiate Transfer E>N > TD E>N Countdown Running > Open Contact 34A > TD E>N Countdown Still Running > After Countdown Transfer Inhibited
  • When 34A Contact Open > Initiate Transfer E>N > TD E>N Countdown Running > After Countdown Transfer Inhibited
  • When 34A Contact Open > Initiate Transfer E>N > TD E>N Countdown Running > Close Contact 34A > Switch successfully retransfer to Normal