Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to do indirect addressing with the M221 in Machine Expert Basic.
Issue:
How to do indirect addressing with a M221.

Product Line:
M221

Environment:
Machine Expert Basic ( formally SoMachine Basic)


Causes and Fixes:
How to

Resolution:
1) open project
2) insert an operate block
3) Enter the following example %MW0[%MW10]:=200
4)  Create an Animation table
5) Enter in the following registers %MW0, %MW10, %MW5, and %MW15
6) Save and build changes
7) For this demo we will use the simulator in Machine Expert Basic to test
8) Load the project in simulator and place in RUN.
9) You will see a value of 200 in the %MW0
10) we will now go to %MW10 and put in the register that we want to move the data to we will enter the value of 5 and also 15 that will reference the %MW5 and %MW15 and it will move thedata of 200 to those registers.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: