How can we help you today?

EcoStruxure Process Expert [2020] Unable to Deploy Supervision Project - Specified Path is not found

This article is used to help the users when facing the below error screenshot while deploying the Supervision.

Specified path not found error

Issue identified in EcoStruxure Process Expert 2020 R2 but is applicable for other versions as well.
In normal project lifecycle when user wants to deploy the supervision project there could be a possibility of the above shown error.

There are 3 major reason for the above error

  1. The IP address of the server is wrong or not available in the network
  2. Aveva Plant SCADA folder was not shared with SoCoDeploy definition and full acces permission was nto given
  3. If the Disk drive is not having enough space.

Schneider Electric Egypt and North East Africa
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
  • Help and Contact Center