Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the Masterpact NW external neutral CT (eNCT) be used on a Masterpact MTZ circuit breaker?
Issue: NW eNCT compatibility with MTZ

Product Line: Circuit Breakers

Environment: Masterpact MTZ

Resolution:
Schneider Electric will not sanction the use of NW ENCT to be used on MTZ because the architecture around the ground is different, and the robustness for EMC and double isolation is different. Use of NW ENCT cannot guarantee unwanted tripping and proper double insulation.