How can we help you today?

Ecostruxure Automation Expert [21.1]: How to read Real Time Clock from Controller.

User can read Real Time Clock from Controller by using a Function block MIBGET. This Function block is available in service section of Runtime.Base library.

MIBGET function block is internally used for getting diagnostic information.

Provide a constant with string 'System.CurrentTime' at Path1. Create a Constant at Q1 and make it True.

pic1

After deployment to Controller, you can see, the block had read the system time and was available at Value1 output.

pic2

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center