Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I set up an Altivar Process drive to close a relay when my motor reaches or exceeds a frequency level?

Issue:
Customer needs a signal when the motor frequency is at or above a setpoint (threshold).

Product Line:
Altivar Process:
ATV630, ATV650, ATV660, ATV680
ATV930, ATV950, ATV960. ATV980
APM

Environment:
All part numbers

Cause:
It's unclear how this function works in the manual

Resolution:
As an Example:  The customer needs a signal from R2A/R2C on the drive to indicate the motor speed is above 30 Hz in order to start other equipment.

  1. under Complete Settings and the Input/Output Configuration; go the the Relay submenu and program the R2 assignment to Mot Freq High Thd (as displayed on the keypad) or Motor frequency high threshold reached (as shown in SoMove).
  2. Under Complete Settings and the Generic Functions menu, go to Threshold Reached and set Motor Frequency Threshold to the setpoint required (30.0 Hz for this example).

When the drive ramps up to 30.0 Hz or higher the R2A/R2C normally open contact will close.
When ramping below 30.0 Hz the relay will actually remain closed until the output frequency goes below 29.6Hz (there is a 0.3Hz deadband when slowing down to prevent rapid cycling of the relay output).

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center