How can we help you today?

EcoStruxure Process Expert: How to remove the warning in simulation control project

This Knowledge base explains the steps to be followed for resolving the warning message popups when the control project is build in simulation mode(when station node is assigned in executable)

The user will be getting the below warning message when he performs the same.

problem

The issue is happening as the ethernet security of EIO bus was not configured as per the requirement.The following steps are needed to be performed to unlock the security of EIO bus in the project

1. Refine the Build project

2. Navigate to the EIO bus configuration as shown below

solution1

3. Navigate to the "Security" tab and click on "Unlock Security"

solution2

4. Save the refine changes

5. Build the project again.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center