How can we help you today?

Ecostruxure Process Expert [2020R2]:How to use "Exec" Function in supervision participant of EPE

This document explains the parameters or settings to be set in Supervision participant to enable the "EXEC" function.

Citect Scada 2018 Supervision participant in Ecostruxure Process Expert 2020 introduced Additional security features, now requires user permission to call the Exec() function.

The user needs to perform the following steps to enable to "EXEC" Function.

1. Open refinement of Supervision Project and Set the Allow Exec field to TRUE for permitted users under Roles in Security.

pic1

2. Add the following parameter in the Citect.ini file

[Security]

BlockExec = 0


This document is applicable for Ecostruxure Process Expert 2020R1 & Ecostruxure Process Expert 2020R2.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center