Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Whether daisy chain of PowerLogic P3 relay with 2 x RJ-45 Ethernet ports work properly or not ? & What is maximum no. device we can connect ?

Issue:
PowerLogic P3 relays with 2 x RJ-45 Ethernet ports.

Environment/Product line:
PowerLogic P3 relay.

Resolution:
Yes ,the daisy chain of Easergy P3 relays with 2 x RJ-45 Ethernet ports should work, up to a maximum of 10 devices.