Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can you create a new project in EcoStruxure Power Build - Easy Series application

Article available in these languages: Vietnamese

Issue: Steps to create a new project in EcoStruxure Power Build - Easy Series
Product Line: EcoStruxure Power Build easy Series
Cause: Need to create a Easy Series Project to manage and configure your product selection
Resolution:
1. Go to the home page of EPB Easy Series
NOTE: It is required to create an account & log in to access the application.
2. Create a new project by clicking on the 'Start' button.

Power Build
3. Enter the required information about the project on the 'Project Information' tab.
Required Information
4. Continue the project by clicking on the 'Save' button or on the 'Switchboards' tab to create a switchboard.
Project Save