How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

What is ASCO 5300 Series ATS Remote Annunciator?

The ASCO 5300 Series enable facility, engineering and maintenance personnel to visually check the status of automatic transfer switches and conduct testing. Locating the annunciator in work areas allows personnel to know the status of transfer switches simply by glancing at the bright green and red LED indicators.

image.png

image.png

Power Requirement, wiring and installation
​​​​​​
Power requirement options:
  • 24V DC supply or
  • 120/220V AC supply​​​​

Wiring Requirement:
  • The power terminals accept 30 to 12 AWG stranded flexible wire.
  • If the power wiring is solid wire, pigtail it with stranded flexible wiring to the ATS Remote Annunciator.
  • Tightening torque for the power terminals is 5 in-lb.

The ASCO ATS Remote Annunciator can be panel mounted or attached to an electrical or masonry gang box.
  • Flush mount or
  • Surface mount
image.png

Communication Wiring:
The communication wiring and ac power wiring must be isolated.
  • Use Belden  1583A cable or
  • equivalent UTP CAT 5e or CAT 6 with RJ-45 connectors (untwisted pair or higher)
  • Two (2) Ethernet ports are available that can be connected to the network or directly to the ATS QEM.
Communications specification:
  • Two 10/100 Base-T (RJ-45) Ethernet ports
  • Half/Full duplex capability

image.png


For more information, refer to these links:
  • Brochure: https://www.ascopower.com/us/en/download/document/PCM-BR-5300PQRTSA/
  • Installation Manual: https://www.ascopower.com/us/en/download/document/ASC-TS-UM-70007ATB7ACTB7ADTB/
  • https://www.ascopower.com/us/en/product-range-presentation/66129-asco-5310-single-channel-remote-annunciator/?parent-subcategory-id=89086
  • https://www.ascopower.com/us/en/product-range-presentation/66130-asco-5350-eight-channel-remote-annunciator/?parent-subcategory-id=89086

Schneider Electric Egypt and North East Africa
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
Help Center

Help Center