Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the main advantage of Bypass-Isolation Automatic Transfer Switch over a standard Automatic Transfer Switch?
The advantage of a Bypass-Isolation Automatic Transfer Switch over the standard Automatic Transfer Switch is that it enables the transfer switch to be completely isolated from the power system and safely tested or serviced without interrupting the power to the loads.  This is done by closing the isolation contacts in series with the transfer switch contacts (closed in normal operation) before opening of the transfer switch contacts. Please see the below operation of the Bypass-Isolation Switch.

Bypass-isolation switches are used in facilities such as healthcare, airports, water treatment plants, data centers, continuous flow industrial processes, correctional facilities, and high-rise office buildings.  When testing or maintenance programs are mandatory such as for facilities where an emergency power system exists, it may not be possible to de-energize the switch for a long period.

Automatic mode
Bypassed to Normal Mode
Test Mode
Isolated Mode


For further information the Application and Design Factors for Automatic Transfer and Bypass-Isolation Switches, please refer to the link below.

Part 1:
https://download.schneider-electric.com/files?p_enDocType=White+Paper&p_File_Name=asc-ts-wp-design-factors-p1.pdf&p_Doc_Ref=TS-WP-DESIGNFACTORS1

Part 2:
https://download.schneider-electric.com/files?p_enDocType=White+Paper&p_File_Name=asc-ts-wp-design-factors-p2.pdf&p_Doc_Ref=TS-WP-DESIGNFACTORS2

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center