Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is Resi9 MP IP41?
Issue:
I need an IP41 Resi9 MP enclosure.

Product Line:
Resi9 MP

Resolution:
Yes, thanks to an additional kit resi9 MP can reach IP41 in both installation, flush and surface.

Notes:
The commercial reference of the IP41 additional kit is MIP99034.
Instruction Sheet BBV48376

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center