This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is 6DL and how is it enabled on the Group G controller?
For automatic units, there is Feature 6DL that can be activated in the Group G controller to require manual retransfer to the Normal source. When activated, the controller will wait for the end-user to press the Transfer button
to complete the retransfer action after the retransfer to Normal time delay has expired. The manual retransfer will be overridden in the event of loss or unacceptability of the Emergency source.
To activate, go to Main Menu --> Settings --> Features --> Feature 6DL and place a check on the tickbox. The default password is 1111.

To activate, go to Main Menu --> Settings --> Features --> Feature 6DL and place a check on the tickbox. The default password is 1111.
Released for: Schneider Electric Egypt and North East Africa