How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

What is ASCO Quad-Ethernet Module (QEM)?

The ASCO 5100 SERIES Quad-Ethernet Modules (QEM) are a line of protocol gateways that provides users with communication interfaces to ASCO transfer switches, meters, and input/output devices.
Embedded webpage with transfer switch annunciation, event logs and remote transfer capabilities
  • Email notification for alert conditions
  • Modbus TCP/IP interface
  • SNMP with trap notifications
  • Four port Ethernet switch functionalities
    • RJ45, 10/100 BaseTX
Control Features
  • ATS Transfer/Re-transfer
  • ATS Timer Bypass
  • Generator Start
  • Generator Test
Monitoring Features
  • ATS and Generator Stats
  • Alarms
  • Voltage and Frequency
  • Statistics and Activity
  • Email Notifications
  • Event Log (300 Events) Optional
  • Monitoring Features
    • Energy Consumption Acc 135L Required
    • Power Demand, Acc 135L Required
Variants
There are two QEM models, the 5140 QEM and 5170 QEM.
image.png

Schneider Electric Egypt and North East Africa