Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Control Expert V15.0 - DTM updates failing due to Security Editor setting
1. Issue
Our customer has come across an issue where he is unable to update the DTM catalogue after installing CE15 software on a Windows 10 PC.
On opening the dummy project (or any other project) the following message pops up:
image.png
Clicking OK causes the DTM audit tool to activate, and the following messages are displayed. Note the message indicating that CE is not installed:
image.png

2. Product Line
ECE V15.0, Security Editor

3. Environment
Win10 Pro 64Bit, ECE V15.0

4. Resolution

We have reproduced this issue by using the same profile as yours, so, we think it's a normal behavior under the SystemOperator selected in Edit profile.

Edit profile - SystemOperator

Based on the test, if selecting Administrator in DTM access rights of Edit profile, it will be able to update the DTM catalog.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: