Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Setting up PID auto/manual for ATV12 drive

Issue:

Setting up PID auto/manual for ATV12 drive

Product Line:

Altivar 12

Environment:

All

Cause:

N/A

Resolution:

Go under CONF, FULL, FUN, PID-, and set PAU to the digital input needed.

Next, set PIN setting to manual reference needed. Options are no, AI1, or A1U1.