Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
CE15,SP1 cannot find the floating license after updating from CE15
If you update Control Expert from 15 to 15,SP1 without updating the Floating License Manager on the Floating License Server, Control Expert will fail to find the floating license.

To resolve the issue, update the Floating License Manager to version 2.6.  The setup file for Floating License Manager version 2.6 can be found in the folder named 'FloatingLicenseManager' on the Control Expert 15,SP1 installation dvd.

It is not necessary to return the license before updating to version 2.6.

image.png