How can we help you today?

What are the minimum and maximum ohm values for braking resistors for the ATV930 drives?

Issue:
Needs ohmic values for ATV930 braking resistors.

Product Line:
ATV930

Environment:
230V up to 75KW, 480V up to 310KW, 600V up to 75KW, 690V up to 90KW.

Cause:
None.

Resolution:
See the attached document showing Min. and Max. ohm values.

Schneider Electric Egypt and North East Africa

Attachment(s)
ATV900_Braking_IE04 600 Volt (1).pdf [412.75 KB]