Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How are the functional marks defined in the Single Line Diagram provided by eDesign Small Building Application
Issue: Defining the functional marks in the Single Line Diagram
Product Line: eDesign Small Building https://edesign-630.se.com/
Cause: Need to tag devices to do the wiring and cabling of the switchboard.

Resolution:A functional mark is generated in the Single Line Diagram for each product whose function is listed below.

It isidentified by a letter indicating the function and a number indicating the position of the device
in the diagram (from left to right and then from top to bottom whatever the function is).

Q : Circuit breaker, Circuit breaker with earth-leakage protection, Fuse
I : Switch, earth-leakage switch, Automatic reset for earth Leakage switch
CT : Contactor
TL : Impulse relay
CTS : BAES
IH : Time switch
IC : Twilight switch
EM : Energy Measurement
PFR : Surge arrestor
X : Socket and other functions

Go to the Diagram tab and select the “SLD View” , under each device you will see a functional mark.