Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Is Sepam 2000 discontinued & what is the replacements for that?
Issue:
Sepam 2000 availability.

Product Line:
Sepam 2000

Resolution:
Yes, Sepam 2000 is discontinued and spare parts are not available to order.
Replacement will be sepam 40/60/80 series or you can use Micom /P3/P5 according to application.

Details can be reachable through our SE site www.se.com.