Issue:
On which terminals are a run contact landed on the S-Flex?
Product Line:
S-Flex
Environment:
Design series E for models with bypass
All models without bypass
Cause:
Hardwiring a run contact
Resolution:
The S-Flex models without bypass use a dry run contact wired between terminals P24 and F. This is a 24Vdc circuit.
The S-Flex models with bypass use a dry run contact wired between terminal 5 and 6. This is a 120Vac circuit and controls Start/Stop when the HOA selector is in the AUTO position.
Released for:Schneider Electric Egypt and North East Africa