Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to power a Can-Open slave threw the SubD9pnt connector of the BMECXM0100?
Description of the problem:
Customers need to know if it's possible to power a can-Open slave connected to the BMECXM0100 master threw the 9-Pin D-SUB Connector?

Here is the Can-Open connector pin assignment of the BMECXM0100 coupler.
3.jpg

We don't provide any specification of an external power supply available on the 9-Pin D-SUB Connector.
The CiA standard reserve pins of CAN connector for power supply but only for transceiver and opto-couplers of physical layer (CiA DR303-1).

Solution:
For providing a power distribution to slaves, a TAP shall have to be add with a possibility to supply the 24V for the power distribution. So you'll have to add an external power supply connected to the TAP.
Sans titre4.jpg

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: