What is the maximum altitude can TeSys Giga contactors be used without derating ?
TeSys Giga contactors can be used up to 5000 meters, and ≤ 3000 meters without any derating.
The derating table on MKTED210011EN for TeSys control contactors is also applicable for the TeSys Giga offer.
The derating table on MKTED210011EN for TeSys control contactors is also applicable for the TeSys Giga offer.
Released for: Schneider Electric Egypt and North East Africa
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
Help Center
Find support resources for all your needs, in one place.