Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PME2020/PME2021 Use my windows credentials fails with "The user name or Password you entered is invalid"

_____________________________________________________________________________________
Section 1 – Product /System/Environment information

PME2020
PME2021
_____________________________________________________________________________________
Section 2 – Issue

Logging in the WebClient Using my windows credentials fails with "The user name or password you entered is invalid"
_____________________________________________________________________________________
Section 3 – Root Cause

If the Windows Authentication setting is disabled in IIS for the default website, the one-click option won't work.

aa

_____________________________________________________________________________________
Section 5 – Troubleshooting/Proposed Solution
Enable the Windows Authentication setting  in IIS for the default website
Reset IIS and the one-click option will work.