This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Is the Breaker Failure (CBF) Start and Trip status available via Modbus in the PowerLogic P3F30 relay?
Issue :
Breaker failure function Start and Trip status availability in MODBUS in Power logic P3F30 relay.
Product line:
Power logic 3F30
Resolution :
Breaker failure function Start and Trip status is available in MODBUS register Stage statuses 406039.
Snap shot attached below for reference.