Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can cause the ATV630 or ATV930 drives ethernet IP address to keep resetting back to all zeros?

Article available in these languages: Japanese

Issue:

IP address keeps resetting back to zeros on the ATV630 or ATV930 drive.

Product Line:

ATV630 ATV930 product lines including enclosed or AFE.

Environment:

All

Cause:

FDR is turned on or the IP mode is not fixed.

Resolution:

The the ethernet settings make sure your are set for Fix IP Mode not DHCP and that FDR (Fast Device Replacement is not turned active)

Also make sure you power cycle the Drive by removing the mains voltage and letting the HMI display to go blank to make sure the IP address is saving.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center