Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
I uninstalled SoMachine 4.x and Machine Expert 1.1, why do I keep receiving an incompatible error message when installing Vijeo Designer SP9?

Issue

When trying to install Service Pack 9 on top of Vijeo Designer an error will appear stating that there is an incompatible version of SoMachine / EcoStruxure Machine Expert installed.

Product Line

Vijeo Designer 6.2, SoMachine 4.0, SoMachine 4.1, SoMachine 4.2, SoMachine 4.3, EcoStruxure Machine Expert 1.0, EcoStruxure Machine Expert 1.1

Resolution

After uninstalling SoMachine and Machine Expert make sure to delete this registry keys if they exist:

HKEY_LOCAL_MACHINE\SOFTWARE\WOW6432Node\Schneider Electric\SoMachine Software

HKEY_LOCAL_MACHINE\SOFTWARE\WOW6432Node\Schneider Electric\Machine Expert Installer

Then reinstall Vijeo Designer 6.2 and apply SP9 as administrator.

Note: SP9 and older is compatible with EcoStruxure Machine Expert 1.2 and up.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: