Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to disable notification area features and virtual desktops from left and right swipe touch function on HMIP6?

On HMIP6xxxxx, to disable notification area features and virtual desktops from left and right swipe touch functions, We can open the Registry Editor, create a new Key named "EdgeUI" under "Computer\HKEY_LOCAL_MACHINE\SOFTWARE\Policies\Microsoft\Windows", then create a new DWORD(32-BIT) Value named "AllowEdgeSwipe",if the value is 0, the function will be disabled, if the value is 1, the function will be enabled.

Please refer to the information in the following picture: