How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

In VAMP 321, What is the next step to be done after physically connecting the arc sensors and the I/O units to the relay?

Issue,
Customer want to know what is the next step to be done after connecting the sensors to the I/O unit

Resolution:
VAMP 321

Environment:
After physically connecting the sensors and the I/O units to VAMP 321 relay, the following steps must be done. These steps are to be done at the beginning of the project installation and repeated after adding or removing any sensor or I/O unit at any time.

1- Make sure you are connected to the relay
2- In VAMPset, Go to Arc protection menu
image 1

3- Go to "Install arc sensors & I/O units " menu and select install.
image 2

4- "Installation state' is then changed from ready to installing
image 3

5- when installation is finished, the installation state will go back to ready.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center